Constant - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Constant folder in the control block palette contains blocks that pass a constant value to block inputs. Constant blocks can have multiple connections to the output of the block. Constant blocks can be any one of the following:

Table 1. Constant Blocks

Block 1

Description

Outputs 2

Constant (Boolean)

Provides a configurable constant value of Boolean type.

Present Value (Boolean)

Constant (Enum)

Provides a configurable constant value of Enumeration (Enum) type.

Present Value (Enum)

Constant (Float)

Provides a configurable constant value of Floating (Float) type.

Present Value (Float)

1 For a constant block, the current Boolean, Enumeration, or Floating value appears in the header of the block.
2 The outputs of this block are exposed for connection by default.