The Activity Outputs folder in the control block palette contains Boolean, float, and enumeration output blocks. Use Activity Outputs to provide an outgoing connection point to custom logic modules.
Note: The tool automatically creates and configures the hierarchy table in a translation block when you connect an Activity Input block to an Activity Output block of a different type (Boolean to two-state Enum or two-state Enum to Boolean).
Type |
Description |
---|---|
Output (Boolean) |
Provides a Boolean output for connections from other blocks in the logic diagram (True or False). |
Output (Enum) |
Provides an enumeration (Enum) output for connection from other blocks in the logic diagram. |
Output (Float) |
Provides a floating (Float) output for connection from other blocks in the logic diagram (numeric value). |