The Reversing Valve Output selections set the logic in the Staged Compressor Control (Heat Pump Staged Compressors v51) Output module to determine whether the Reversing Valve Outputs (REV1-C and REV2-C) should be commanded on when there is a call for heating or cooling.
The selection options for Reversing Valve Output(s) are:
-
On for Cooling
-
On for Heating