Monitored Safeties (FC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Discharge Air Smoke Detector option creates an Input that is mapped to the supervisory system to create an alarm point.