Proportional (FC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Proportional: Select this option if the coil is controlled by a proportional valve that takes a 0–10 VDC or 4–20 mA signal.