This option allows the unit to shut down based on the energy hold off Network Input. If Energy Hold Off Switch is selected in the Misc (FC) section, then the Network Input or the Hardware Input (BI) can activate the mode. This feature is typically used to shut down the temperature and airflow control when a window or loading door is open (for example, a window switch).