Power Fail Restart Logic (FC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This option creates the interface for the supervisory system scheduling logic.

Override Support creates the local override interfaces from optional Occupancy Sensors or Networked Sensor Temporary Occupancy interfaces.