Fan Status Interlock with Zone Heating (FC) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This option is available only if a Stage Heating Coil is selected. When selected, logic is created to monitor fan status through a binary input. The Airflow Status Determination (Flow Status Determination) module uses this status feedback to enable or disable the Staged Heating Control (Heating Staged Outputs v51) Output Controller.