This option is available only if a Stage Cooling Coil is selected. When selected, logic is created to monitor fan status through a binary input. The Airflow Status Determination (Flow Status Determination) module uses this status feedback to enable or disable the Staged Cooling Control (Cooling Staged Outputs v51) Output Controller.