Point Assignment Tab - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

See the Defining Hardware section.

Note: SA Bus devices are not part of the point assignment process. See Modifying Points on an SA Bus Device.
Table 1. Hardware Definition - Point Assignment Tab

Field

Description

Unassigned Points

Displays all the unassigned points. The object names appear alphabetically.

  • Name: Displays the point name.
  • Description: Expanded ID for the point.
  • Signal: Displays the signal information.
  • Data Type: Data type.
  • Type: Displays the type information.

Assigned Points

Displays all the assigned points. The object names appear alphabetically, including the Object Name, Expanded ID, Signal, Data Type, and Type.

  • Controller Label: Controller information.
  • Name: Displays the point name.
  • Description: Expanded ID for the point.
  • Signals: Displays the signal information.
Note: Select a point and use drag-and-drop functionality to move a point up or down on the list. An alert message appears if you attempt to move the point to an invalid location and the point remains in its original location.

Moves the selected point (or points) from the Unassigned Points table to the Assigned Points table.

Moves the selected point (or points) from the Assigned Points table to the Unassigned Points table.

Close

Closes the dialog box.

Opens the Help system.