See the Defining Hardware section.
Field | Description |
---|---|
Slider Bar (1 to 5) | Use to set the maximum quantity of devices that appear in the quantity slider bar of the Add Devices dialog box. |
OK | Applies the changes and closes the dialog box. |
Cancel | Closes the dialog box without applying the changes. |
Opens the Help system. |