Add Devices Dialog Box (For I/O Modules) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

See the Defining Hardware section.

The Add Devices dialog box appears after you select an I/O Module device to add in the SA Bus Device Selection dialog box. Use this dialog box to name your device.

Table 1. Add Devices Dialog Box (For I/O Modules)

Field

Description

Device Name

Device name.

Quantity

Use to select the number of I/O modules (see Set Maximum Quantity Dialog Box).

Starting Index

Use to enter the starting index for the I/O Modules you are adding to your system.

OK

Applies the changes and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.

Opens the Set Maximum Quantity Dialog Box.