See the Defining Hardware section.
Field |
Description |
---|---|
Field Device |
Name of the device. |
Select |
Opens the Field Device Selection Dialog Box to select the device. |
SA Bus Devices |
Lists all the SA Bus Devices assigned to the Field Device. |
Add Device |
Opens the SA Bus Device Selection Dialog Box to select your SA Bus device. |
Delete |
Deletes the selected device from the SA Bus Devices field. |
ModifyDevice |
Opens the Modify Points dialog box to add points to your SA Bus device. Note: You can only add points to an SA Bus device if the device is a Network Sensor (Network Duct Sensor, Network Zone Sensor, or Network CO2 Sensor), Wireless Refrigerator/Freezer Temperature Transmitter and Probe Assemblies (Network Cooler/Freezer Sensors), Wireless Sensor (Network Zone Sensor), or a Network VSD.
|
Hardware Slot Summary |
Requirements of the system you select. The Hardware Slot Summary displays the hardware requirements of the system in the CAF, the hardware capacity of the selected devices (Selected Hardware), unused space, and available space (Unused/Available Space). When the CAF exceeds the capacity of the selected hardware, the field turns red to indicate an additional hardware device is needed to support System Selections. Category: System Requirements, Selected Hardware, and Unused and Available points. The Hardware Slot Summary is the summary of points prior to mapping all points. The Hardware Slot Summary includes the following types:
For information on signal types used by these points, see Object Naming and Signal Preferences. |
Close |
Closes the dialog box. |
|
Opens the Help system. |