Package Check at Startup - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
About this task

The tool automatically checks for new or updated firmware package files at system start-up. These files are stored in the Packages Directory: C:\ProgramData\Johnson Controls\MetasysIII\Field Controller Packages.

The tool uses the newest version of a package file for a given release.

For example, if you have a Release 6.1 package for an Advanced Application Controller and place a patched Release 6.1.1 file in the Packages Directory, then the tool automatically installs the 6.1.1 patch package files at system startup, and replaces your 6.1 file.

Note: Do not place new package files in the Packages Directory. Instead, follow the steps outlined in Reviewing Available Packages.