Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
About this task
Use the Import feature to import packages.
Procedure
Click Define Hardware.
On the Packages tab, click Import, and then navigate to the package file that you want.
Note: Field controller packages show the status Licensed or Unlicensed in the Packages tab. If a field controller package is unlicensed, the CAF can be opened as pseudo-artificial.