About this task
The Point Assignment screen appears when you select the Point Assignment tab in the Define Hardware dialog box. See Selecting a device (Controller Selection tab).
The tool automatically assigns the points based on the selections made in the Controller Selection tab. Points that it could not assign appear in the Unassigned Points list. You need to assign the points in the Unassigned Points list.
Note: SA Bus devices are not part of the point assignment process. See Modifying Points on an SA Bus Device.
You must have an application (CAF file) open to assign points.
Note: You may also need to reassign points after you change hardware. If you change hardware, verify that your point assignments have not changed.