Modules (Custom/Monitoring Pipe Mounted Items) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Pipe Mounted Items selections load the following modules in this Control View column:

Inputs

  • BLDGX-L (Bldg X Load AI, where X is 1-6): This Input is loaded when the BTU Meter (AI) node is selected. Specific Inputs are loaded per BTU meter.

  • FLOWX-S (Flow Status X BI, where X is 1-6): This Input is loaded when the Water Flow Status Switch (BI) node is selected. Specific Inputs are loaded per switch.

  • PIPEX-F (Flow Input X AI, where X is 1-6): This Input is loaded when the Water Flow Sensor (AI) node is selected. Specific Inputs are loaded per sensor.

  • PIPEX-P (Pipe X Pressure AI, where X is 1-6): This Input is loaded when the Water Pressure (AI) node is selected. Specific Inputs are loaded per sensor.

  • PIPEX-T (Pipe X Temperature AI, where X is 1-6): This Input is loaded when the Temperature Sensor (AI) node is selected. Specific Inputs are loaded per sensor.

  • STM-P (Steam Pressure AI): This Input is loaded when the Steam Pressure (AI) node is selected.

See the Input Modules section.