Modules (Custom/Monitoring Natural Gas Items) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Natural Gas Items selections load the following modules in this Control View column:

Inputs

  • NG-F (Natural Gas Flow AI): This Input is loaded when the Monitor Flow Sensor (AI) node is selected.

  • NG-P (Natural Gas Pressure AI): This Input is loaded when the Monitor Pressure Sensor (AI) node is selected.

  • NG-S (Natural Gas Pressure BI): This Input is loaded when the Monitor Pressure Switch (BI) node is selected.

See the Input Modules section.