The Misc Status Items selections load the following modules in this Control View column:
Inputs
-
DOORX-S (Door X Status BI, where X is 1-6): This Input is loaded when the Monitor Door Switch (BI) node is selected. Specific Inputs are loaded per switch.
-
MOTOR-S (Motor Status BI): This Input is loaded when the Motor Status (BI) node is selected.
-
SMKX-S (Smoke Detector X Status BI, where X is 1-6): This Input is loaded when the Monitor Smoke Detector (BI) node is selected. Specific Inputs are loaded per smoke detector.
See the Input Modules section.