Misc Status Items (Custom/Monitoring) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The selection options for Misc Status Items are:

  • Motor Status (BI): This option indicates whether a motor is running.

  • Monitor Smoke Detector (BI): This option indicates whether the system is in an alarm condition due to the detection of smoke for up to six locations.

    • 1 Point (1 BI)

    • 2 Points (2 BIs)

    • 3 Points (3 BIs)

    • 4 Points (4 BIs)

    • 5 Points (5 BIs)

    • 6 Points (6 BIs)

  • Monitor Door Switch (BI): This option indicates the open/closed status of a door to a room or control cabinet for up to six locations.

    • 1 Point (1 BI)

    • 2 Points (2 BIs)

    • 3 Points (3 BIs)

    • 4 Points (4 BIs)

    • 5 Points (5 BIs)

    • 6 Points (6 BIs)