Misc Alarm Monitoring (Custom/Monitoring) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The selection options for Misc Alarm Monitoring are:

  • Fire Alarm Inputs: These options indicate whether the fire alarm system (fire control panel and Halon equipment) is in an alarm or trouble condition.

    • Monitor Panel Alarm (BI)

    • Monitor Panel Trouble (BI)

    • Monitor Halon Alarm (BI)

    • Monitor Halon Trouble (BI)

  • Monitor Refrigerant Alarm (BI): This option indicates whether the refrigerant system has a leak.

  • Monitor Gas Detection (BI): This option indicates whether the system detects a gas leak.

  • Compressed Air Low Pressure Switch (BI): This option indicates whether the compressor is in an alarm condition due to low pressure.

  • Monitor Chemical Treatment Alarm (BI): This option indicates whether the chemical treatment system is in an alarm condition (for example, due to a leak).

  • Monitor Sump Pump Alarm (BI): This option indicates whether the sump pump system is in an alarm condition (for example, due to a high sump level) for up to six pumps.

    • 1 Point (1 BI)

    • 2 Points (2 BIs)

    • 3 Points (3 BIs)

    • 4 Points (4 BIs)

    • 5 Points (5 BIs)

    • 6 Points (6 BIs)

  • Monitor Sewage Pump Alarm (BI): This option indicates whether the sewage pumping system is in an alarm condition for up to six pumps.

    • 1 Point (1 BI)

    • 2 Points (2 BIs)

    • 3 Points (3 BIs)

    • 4 Points (4 BIs)

    • 5 Points (5 BIs)

    • 6 Points (6 BIs)

  • Moisture Detector (BI): This option indicates whether the system is in an alarm condition as a result of moisture levels for up to six locations.

    • 1 Point (1 BI)

    • 2 Points (2 BIs)

    • 3 Points (3 BIs)

    • 4 Points (4 BIs)

    • 5 Points (5 BIs)

    • 6 Points (6 BIs)

  • Panic Button (BI): This option indicates whether a panic button set off an alarm condition for up to six locations.

    • 1 Point (1 BI)

    • 2 Points (2 BIs)

    • 3 Points (3 BIs)

    • 4 Points (4 BIs)

    • 5 Points (5 BIs)

    • 6 Points (6 BIs)

  • Monitor Emergency Shuttoff (BI): This option indicates an alarm condition due to an emergency shutoff for up to six systems.

    • 1 Point (1 BI)

    • 2 Points (2 BIs)

    • 3 Points (3 BIs)

    • 4 Points (4 BIs)

    • 5 Points (5 BIs)

    • 6 Points (6 BIs)

  • Water Tank Low Level Alarm (BI): This option indicates whether the water tank is in an alarm condition due to a low water level.

  • Water Tank High Level Alarm (BI): This option indicates whether the water tank is in an alarm condition due to a high water level.

  • Water Tank Level Sensor (AI): This option monitors the water level in the water tank.

  • Monitor Earthquake Detector (BI): This option indicates whether the system is in an alarm condition due to the detection of an earthquake.