Modules (Custom/Monitoring Generator Items) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Generator Items selections load the following modules in this Control View column:

Inputs

  • GEN-A (Generator Alarm BI): This Input is loaded when the Monitor Alarm (BI) node is selected.

  • GEN-LVL (Generator Fuel Level AI): This Input is loaded when the Monitor Fuel Level (AI) node is selected.

  • GEN-S (Generator Status BI): This Input is loaded when the Monitor Status (BI) node is selected.

  • GEN-TBL (Generator Trouble BI): This Input is loaded when the Monitor Trouble (BI) node is selected.

See the Input Modules section.