The Duct Items selections load the following modules in this Control View column:
Inputs
-
DUCT-P (Duct Pressure AI): This Input is loaded when the Duct Pressure Sensor (AI) node is selected.
-
DUCTX-T (Duct X Temperature AI, where X is 1-6): This Input is loaded when the Duct Temperature Sensor (AI) node is selected. Specific Inputs are loaded per sensor.
-
FILTX-S (Filter X DP Alarm BI, where X is 1-6): This Input is loaded when the Filter Status Diff Pressure Switch (BI) node is selected. Specific Inputs are loaded per switch.
-
HP-A (Duct High Static Fault BI): This Input is loaded when the High Duct Pressure Switch (BI) node is selected.
-
HT-A (High Temperature Limit Fault BI): This Input is loaded when the High Duct Temperature Alarm (BI) node is selected.
-
LP-A (Duct Low Static Fault BI): This Input is loaded when the Low Duct Pressure Switch (BI) node is selected.
-
LT-A (Low Temperature Limit Fault BI): This Input is loaded when the Low Duct Temperature Alarm (BI) node is selected.
See the Input Modules section.