Modules (Custom/Monitoring Domestic Water Items) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The Domestic Water Items selections load the following modules in this Control View column:

Inputs

  • DHW-A (Domestic HW Temp Alarm BI): This Input is loaded when the Monitor Domestic HW Alarm (BI) node is selected.

  • DHW-T (Domestic HW Temp AI): This Input is loaded when the Domestic HW Temp Sensor (AI) node is selected.

  • DHWP-S (Domestic HW Pump Status BI): This Input is loaded when the Monitor Domestic HW Pump (BI) node is selected.

  • DWP-S (Domestic Water Pump Status BI): This Input is loaded when the Monitor Domestic Water Pump (BI) node is selected.

See the Input Modules section.