Domestic Water Items (Custom/Monitoring) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The selection options for Domestic Water Items are:

  • Domestic HW Temp Sensor (AI): This option measures the temperature of the domestic hot water system.

  • Monitor Domestic HW Alarm (BI): This option indicates whether the domestic hot water system is in an alarm condition.

  • Monitor Domestic Hot Water Pump (BI): This option monitors the domestic hot water pump.

  • Monitor Domestic Water Pump (BI): This option monitors the domestic water pump.