Modules (Custom/Monitoring Voltage Output) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Voltage Output selections load the following modules in this Control View column:

Outputs

  • VOLTX-O (Voltage Out X AO, where X is 1-6): This Output is loaded when the Voltage Output (AO) node is selected. Specific Outputs are loaded per sensor.

See the Output Modules section.