Command Motor (Custom/Monitoring) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The selection options for Command Motor are:

  • Command Motor (BO): This option indicates the command to the motor.

    • Status (BI): This option indicates whether the motor is running based on the motor command for up to six motors.

    • Quantity

      • One

      • Two

      • Three

      • Four

      • Five

      • Six