Custom and Monitoring Supervisory Control Only Applications - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The Custom applications and Monitoring Supervisory Control Only applications provide general point monitoring inputs and other miscellaneous outputs. The Mechanical System Selection includes general point monitoring options, such as points for temperature sensors located in ducts, and options to monitor alarms or status for generators, medical gas, and other important systems. The Control Logic Selection includes miscellaneous outputs, such as outputs to command motors, lighting, two-position actuated devices, or other equipment, and options for current and voltage outputs for modulating system devices.

You can view preferences and modify any default signals associated with the inputs or outputs created using the System Selection wizard. Appropriate hardware and filter setup default view parameters have been established for each input or output.

Note: Custom applications are intended for use with Field Controllers, and Monitoring Supervisory Control Only applications are targeted for I/O Modules. Keep in mind that Monitoring Supervisory Control Only applications do not allow you to add any other modules; only inputs and outputs.
Note: The Custom applications and Monitoring Supervisory Control Only applications currently provide the same options, and are described together in this section of the Help system. One exception is that when you select Wind Direction in the Outdoor Air Items section for Custom applications, the Wind Direction Determination module appears in addition to the WIND-DIR input. For Monitoring applications, only the WIND-DIR input appears.