Specifying Local Controller Display settings - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Procedure

  1. Start the tool and open the controller application.
  2. Select the Display widget.
  3. Click Edit.
  4. Locate the Display Setup panel.
  5. In the Display area, click the drop-down box to select a Contrast level value.
  6. In the Display area, click the drop-down box to select a Backlight Intensity setting value.
  7. Click Apply. The display configuration is saved. This change becomes effective after you transfer the application to the controller. See Transferring the Application of the Display Device.