System Tree Panel - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The System Tree panel allows you to view, in a tree format, the parameters exposed for BACnet systems.

When you are not in Edit mode, the System Tree panel functions like the BACnet Exposed widget; you can view system folders and points, and use Mass Edit without leaving the Display Widget. The names of the points, objects, and the structure of the tree update if changes are made to the application.

When you are in Edit mode, the System Tree functionality is limited, and you cannot mass edit System Tree points. In Edit mode, the controller display can be configured by moving the System Tree folders and points to the Display Pages panel.

Table 1. System Tree Panel

Field

Description

Apply

Applies the changes and exits the Edit mode.

Cancel

Exits Edit mode without applying the changes.

Settings

Show All: Displays all points.

Show BACoids: Displays the points that are BACnet Exposed.

Show Description: Displays descriptions of the points that appear in the tree.

Filter

Filters all folders and points on the tree to match the entered text.

Tools

BACnet Exposed Count: Number of BACnet Exposed points.

Mass Edit Dialog Box: Use to filter on a name, show all points, show only BACnet Exposed points, show only hardware points (control points, sensors, and miscellaneous points), show duplicate points, and edit values. See Mass Edit Dialog Box.

Expansion Level

Indicates the level of details that appear within the tree (1 to 5).