The Display Pages panel allows you to configure the Idle, Inputs and Outputs, Parameters, and User Defined pages that you see in the display.
Field |
Description |
---|---|
Apply |
Applies the changes and exits the Edit mode. |
Cancel |
Exits Edit mode without applying the changes. |
DIS1710 |
Auto Populate: Automatically fills in the display
configuration for compatibility with the local controller display.
Note: Auto Populate may also be used for the MAP Gateway. In this
case, you can rename any folder and add any amount of User Defined pages to the
display.
Tool Tip: Displays folder expectations for local controller display compatibility, including:
|
Create Page |
Creates a new folder at the bottom of the tree. For any setup apart from local controller displays, you can customize the configuration completely by adding new folders and copying System Tree points to the Display Configuration tree. |
Import/Export |
Import: Imports an XML or CAF file from any folder. Export: Exports an XML file to any folder.Note: You must click Apply to save your configuration before exporting a file.
|