Display Configuration - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

You can customize what information displays in the MAP Gateway UI or on the local controller display.

For MAP Gateway, the Display widget allows you to:

  • define which folders and points appear on the home page

  • define the order and groupings of folders and points on the home page
  • edit point user names and descriptions using the Mass Edit feature

After you configure the display, transfer the application to the controller, and then click Rediscover Devices in the MAP Device List page. The MAP Gateway is alerted and reads the new display information.

For Local Controller Displays, the Display widget allows you to:

  • define which folders and points appear on the display panel (Idle, Inputs and Outputs, Parameters, and on User Defined pages that you see in the display)

  • define the order and groupings of display panel folders and points
  • automatically populate pages with points
  • define which points are read-only (cannot be commanded using the display)
  • edit point user names and descriptions using the Mass Edit feature

  • set display attributes including contrast and backlight intensity

  • select timeout settings

  • select authorization including password definition

After you configure the display, transfer the application to the controller. The changes then become effective.

Note: From Release Mode 10.6, the DIS1710 is displayed but works with any display compatible with this feature.