Important: If you have already selected a system or opened a CAF in the tool, you can
view and change the selections made. All previous user modifications are lost if you make
changes to the system selections (lost changes include: sideloops, user added inputs,
outputs, network inputs, network outputs, modules, changes in state tables, parameters,
logic, and input/output setup). For information on the types of systems and selections
available, see the User Interface and Applications sections.
See Rerunning System Selection in the Upgrading System Files section for guidelines on viewing and modifying system selection.