Setting the Actuator Stroke Time - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
About this task

The following procedure defines the proper method for setting or changing the actuator stroke time for a VAV Single Duct or VAV Dual Duct damper PAO. For all other PAOs, edit the stroke time through the Details dialog box.

To set the Actuator Stroke Time:

Procedure

  1. Using the Setpoint/Miscellaneous Modules category, right-click the Supply Damper Stroke Time, Hot Deck Damper Stroke Time, Cold Deck Damper Stroke Time, or Exhaust Damper Stroke Time module and select View Details. You also can double-click the module to open the Details dialog box. The Details dialog box appears.
  2. Click Edit.
  3. Adjust the default value of the output.
  4. Click Apply.
  5. Click Close.
    The stroke time change is fed to all of the modules connected to the changed module.