Using the Activities Tree - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Activities tree appears at the top of the left panel in the logic view.

To view the logic of the entire application, click the Control View Connections option (appears second in the list, just below the Activities folder). The logic of the entire application appears in the right panel of the logic view. The Control Block Palette does not appear when the Control View Connections option or a module category folder (for example, Output Control) is selected.

Note: By default, the Control View Connections option is selected when you view Logic.

To view the logic of a particular module, browse the folders of the Activities tree (organized by module category) and click the module, or right-click the module and select View Logic. The logic diagram of the module appears in the right panel and the Control Block Palette appears below the Activities tree in the left panel.