Printing the Logic Diagram - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

See the Logic Tab Screen description in the User Interface section.

For information on printing summary reports, see Printing Summary Reports in the User Interface section.

To print the logic diagram:

Print Preview

Click the Print Preview button in the Logic View toolbar. The Print Preview screen appears with the following options:

  • Print Setup

    Note: The Print Setup dialog box contains a Page Setup button that allows you to change the orientation of the page from Portrait to Landscape and vice versa.
  • Print

  • Zoom In

  • Zoom Out

  • Fit In Window

Print

Click the Print button in the Logic View toolbar. The Print dialog box appears. Select the desired print settings and properties and click OK.