Panning - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
About this task

See the Logic Tab Screen description in the User Interface section.

To pan in the logic diagram:

Procedure

  1. Click the Pan Canvas Tool () icon in the Logic View diagram vertical toolbar.
  2. Click and hold the pointer down while moving the mouse.
  3. Release the hold when you reach the desired location.
    Note: You also can use the plus (+) and minus (-) keys to zoom in and out, and the arrow keys move up, down, left, or right. You can also use the scroll wheel to move up and down, hold the Shift key and scroll to move left and right, and hold the Ctrl key and scroll zoom in and out.