Exposing Ports - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

About this task

You can expose ports to make them available for connection. If you expose ports for BACnet systems, the BACnet exposed ports are viewable objects through the Supervisory Controller. You cannot remove the selection for connected ports because the ports are disabled in the Port Exposure dialog box.

To expose ports for BACnet systems using the Details dialog box:

  1. Right-click a block and select View > Details. The Details dialog box appears. See the Details Dialog Box and Viewing and Modifying Details sections.
  2. Click Edit.
  3. For the BACnet Exposed selection, select True.
  4. Click Apply.
  5. Click Close.