Copying a Block - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
About this task

When you copy a block, you can paste the block into the same state section or activity of the copied block, or a different state section or activity.

Procedure

  1. Right-click the block and select Copy. To copy multiple blocks at once, press and hold the Ctrl key while selecting each item, and then select Copy. When you select multiple blocks, the associated connections are also copied.
  2. Right-click within the logic diagram and select Paste.
    Note: You also can select a block and use the Ctrl-C and Ctrl-V keys to perform the copy and paste function.