About this task
You can duplicate ports using the Clone Ports dialog box. Only ports that are exposed and non-connected can be duplicated. See the Clone Ports Dialog section.
Specific properties of the ports are copied, depending on which type of port you clone:
- Enum type - name, default value, and states text
- Boolean type - name, default value, active text, and inactive text
- Float type - name, default value, units, and display precision
Note: The Clone Ports dialog is not available for Activity Input or Activity Output blocks, with the exception of the State block of a Hybrid Activity.
To clone a port: