Procedure
- Click the State Tables tab. The State Tables tab appears with the system’s state selection data populated within tables in the right pane, and the states in the left pane of the tab. The panes allow you to scroll both vertically and horizontally, keeping the first column visible. See the State Selection (State Tables Tab) screen section.
- Click Edit.
- Right-click the module name and select Change Table Label (a yellow table heading indicates a connected module, whereas an orange table heading is a module that is not connected). The Rename/Name dialog box appears.
-
Type a name in the Name field.
Note: We recommend leaving the label field empty so that dynamic naming may be used.
- Click OK.
- Click Apply.