Select Reference Dialog - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
See Making a Connection and Changing a Connection.

Table 1. Select Reference

Field

Description

Filter Provides text box to search the selection tree based on the node name. The search results include the matching node and its ancestors.

Left Pane

Shows available modules within the system tree.

Right Pane

Lists the input/output ports to which you can connect.

OK

Applies the changes and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.