This dialog box is used to make changes to the labels in the State Tables. See Customizing State Selection Tables.
Field |
Description |
---|---|
Name |
Use to type a name for the input. We recommend leaving this field empty so that dynamic naming may be used. |
OK |
Applies the changes and closes the dialog box. |
Cancel |
Closes the dialog box without applying the changes. |
|
Opens the Help system. |