Mode Selection - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

See Configuring the MUX Block.

Table 1. Mode Selection

Field

Description

Mode

Use to select a value to use for the input mode of a MUX block.

OK

Applies the changes and closes the dialog box.

Cancel

Closes the dialog box without applying the changes.

Opens the Help system.