See Configuring the Line Segment Block.
Field |
Description |
---|---|
Edit | Use to edit the table data. |
Name | Use to enter a name for the block. |
Object Identifier | Indicates object BACnet ID and instance number. |
Input and Outputs Table |
Displays both an Inputs and an Outputs table for the selected module/block. These tables include the following data:
|
Input Points |
Lists the values expected of the Line Segment input in ascending order. |
Output Points |
Lists the values that the Line Segment maps to from the Input Points column. |
Apply |
Applies the changes. |
Cancel |
Discards the changes. |
Close | Closes the screen. |
|
Opens the Help system. |