Configuration - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
In Configuration mode, you can add, remove, and modify the contents of your system. For example, you can add an input and define state generators. You can also modify your system’s control logic. You can connect inputs and outputs, add and remove logic blocks, and expose ports. See the Setting Preferences Steps section for details on how to perform the configuration tasks. See the User Interface section for a description of the user interface and its contents.

Once a system is selected and configured using the System Selection Wizard, the modules and logic provided control your system as expected. Only modify logic if you require a unique control that the System Selection Wizard did not address.