Adding a Broadcast Management (BBMD) Object - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

About this task

If you open a CAF file that does not have a Broadcast Management object defined, you can add an object using one of the following methods:
  • Click on the Device Information folder and press Insert.
  • Right-click the Device Information folder and select Add BBMD Configuration.
  • Click Select in the Field Device section in Define Hardware. If the selected field device supports BBMD functionality, it appears in the Advanced tab.
  • In the Transfer Summary screen, select an option in the BBMD Enabled list and then select Modify open application with New Information column. The Broadcast Management object appears when the transfer process is complete.