Adding a Trend - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

About this task

A trended item is a data point in the controller that is periodically sampled and logged. You can view trend logs in table or chart format. To view trend samples, you need to be in Commissioning mode.

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab.
  3. In the Advanced Object tree, right-click Trends and then click Add Trend. A new trend is added to the Advanced Object tree.
  4. Select the trend and then click Edit. The fields you can edit appear in white.
  5. Enter information for the trend. See Trend Details Screen.
  6. Click Apply.