About this task
Procedure
- Start the tool and open the controller application.
- Click the Advanced tab. The Device Information folder and information screen appear.
- Under the Device Information folder, select the controller you want to view. Information about the controller appears in the right section of the screen.
- Click Edit. The fields that you can edit appear in white.
- Edit the parameters of the device. See Device Information Screen.
- Click Apply.