Field |
Description |
---|---|
Object - Name |
Indicates the name of the schedule. |
Description |
Indicates the description of the schedule. |
Enabled |
Indicates if the schedule is enabled (True) or disabled (False). |
Object Identifier |
Indicates the read-only ID of the schedule. |
BACnet - Priority for Writing |
Indicates the priority of the schedule. The lower the number, the higher the priority. |
Operation and Display - Effective Period |
Indicates the time frame that the schedule is in effect. Click the browse button to define this information. |
Schedule Output Type |
Indicates the output type of the schedules: Binary, Analog, and Multistate. |
Default Schedule Command |
Indicates the default text that appears when you create the schedule: Release (Binary, Analog, Multistate), Off, or On. Note: If the Default Schedule Command is set to Release, the scheduling feature’s control over the scheduled items ends. Release should only be used for the Default Schedule Command if the scheduled items support the Release command.
|
States Text |
Indicates the state text options used when you view and create the schedule. |
Display Mode |
Indicates the available schedule display modes: Weekly Schedule, Exception Schedule, and Exception Items. |